|
ARD2
1.00 for Rev B. Hardware
Airbag Reference Demonstrator using MPC5604P
|
Establishes a relationship between the SBC and the peculiarities of PSI5 sensors. More...
Functions | |
| uint16_t | u16fnMMA5100TreatData (uint16_t *pu16SatData, uint8_t *pu8ResultArray, uint8_t *pu8CurrentIndex, uint8_t *pu8IndexAdder, uint32_t *pu32AlreadyWritten) |
| As PSI5 satellite data comes in, this function treates the currently received word and gets ready to treat it. It shall be called several times in order to take care of all downloaded data. | |
Establishes a relationship between the SBC and the peculiarities of PSI5 sensors.
Copyright (C) 2011 Freescale Semiconductor Freescale Confidential Proprietary
History:
| uint16_t u16fnMMA5100TreatData | ( | uint16_t * | pu16SatData, |
| uint8_t * | pu8ResultArray, | ||
| uint8_t * | pu8CurrentIndex, | ||
| uint8_t * | pu8IndexAdder, | ||
| uint32_t * | pu32AlreadyWritten | ||
| ) |
As PSI5 satellite data comes in, this function treates the currently received word and gets ready to treat it. It shall be called several times in order to take care of all downloaded data.
| pu16SatData,: | Pointer to the current word that has been received. |
| pu8ResultArray,: | Pointer to a memory location that shall contain an array where to store all registers; a virtual memory map, if you will. |
| pu8CurrentIndex,: | Pointer to a memory location that keeps track of the current index for the next piece of data. |
| pu8IndexAdder,: | Pointer to a memory location that shall remember if we have already downloaded the first half of the register table, and if we have, writes to it to generate an index offset used in the pu8ResultArray. |
| pu32AlreadyWritten,: | Pointer to a mask that keeps track if an existing register has already been written or not. |